Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
ESD-Slide4

There are 3 types of ESD: Sparks – A spark is triggered when the electric field strength exceeds approximately 4-30kV/cm. This may cause a very rapid increase of free electrons and ions in the air, temporarily causing the air to abruptly become an electrical conductor. Corona discharge – A corona discharge occurs between a highly curved electrode and an electrode of low curvature. Brush discharge – A brush discharge occurs between an electrode with a curvature between 5-50mm and a voltage of about 500kV/m. The resulting discharge paths have the shape of a brush.

PTM פורסם ב: