Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
ESD-Slide9

The Charged Device Model (CDM) test simulates how the device acts when the device itself has an electrostatic charge and the effects of the discharge when it comes in contact with a metallic surface. This type of discharge is the most common type of ESD in electronic devices and is the main cause of ESD damage during the manufacturing process. CDM discharge depends mainly on parasitic parameters of the discharge and is strongly dependent on the size and type of component package.

PTM פורסם ב: