Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Industrial-Ethernet-Slide10

The M12 family has many variations, and thus to minimize incorrect mating of similar looking connectors on a panel, they are coded so that only like-coded connectors actually mate. The most common is “A” code, which originally had four or five contacts. This has been extended to twelve, with eight contacts becoming a standard for industrial Ethernet at 1Gbps speeds. For common factory floor speeds of 10/100, the “D”’ code is used. In addition to the insulator coding, “D”’ code connector insulators are often colored green.

PTM פורסם ב: