Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
CJS-CAS-Slide2

Here are some of the features of Copal Electronics’ slide switches. First is the self-cleaning contact mechanism. The wiping action of the contact removes foreign particles from the surface of the contact. Gold-plated contacts are available in all of Copal’s slide switches. Using adequate heat-resistant resin in each part of the slide switch enables the switch to withstand the high temperatures required in Pb-free soldering.

PTM פורסם ב: