Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
inverter-slide13

This plot shows the improvement in radiated EMI between the unit with Si PiN diodes and SiC Schottkys. The purple line is the limit line under which the spectrum must be maintained in order to pass this particular standard. Note the dramatic improvement between 30MHz and 110MHz with SiC technology.

PTM פורסם ב: