Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
inverter-slide6

These waveforms represent diode switching characteristics taken from a working inverter circuit. Note the large reverse recovery current in the Si PiN device. The recovery peak current is almost 19A with a recovery time of 141ns. The Wolfspeed SiC example shows elimination of the recovery current showing only a small capacitive loss that is independent of temperature. 

PTM פורסם ב: