Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
XB-D White LEDs Slide 12
Another design example where the XB-D is particularly effective is the PAR38 lamp. In this limited space, an engineer can use 12 XB-D LEDs and achieve 1300 lumens. On the other hand, given the same space constraint only 6 of competitor #1’s LEDs and 7 of competitor #2’s LEDs can be used and would result in considerably less lumens as can be seen on this page. In addition, the small form factor of the XB-D enables the use of one reflector which is not possible using other LED solutions. Using one reflector enables engineers to achieve an appearance more like a conventional filament. It also reduces multiple shadows in the light beam and reduces the number of optics used which results in lower total system cost and improved appearance.
PTM פורסם ב: