Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
CCHD-957-slide3

Examining the close-in performance of the 22.5792MHz oscillator, it can be seen that the phase noise at 10 Hz is -97.3dBc/Hz. This represents a significant improvement over traditional clock oscillators. The data indicates that the noise floor at 1MHz is -169.69dBc/Hz. To obtain phase noise performance in this range would normally require the use of a much more expensive oscillator.

PTM פורסם ב: