Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
CUI Devices Peltier - Slide11

The combined effect of the thermally conductive resin and the SbSn solder joints within the arcTEC™ structure has a dramatic effect on the reliability and life span of the Peltier modules. The data shows the stark contrast between Peltier modules built with and without the arcTEC™ structure. After as few as 3000 thermal cycles, the conventional Peltier modules already show a dramatic change in resistance. In contrast, the modules built using the arcTEC™ structure show negligible change in resistance all the way out to 30,000+ thermal cycles.

PTM פורסם ב: