Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
ez-ble cyble cyble-022001-00 datasheet cyble-222005-00 datasheet cyble-222014-01 datasheet proc ble datasheet getting started application note psoc creator psoc programmer cysmart windows host emulation tool cysmart ios and android apps

This slide is a solution summary of the module. It is a broad application solution. Almost every industry including consumer, medical, and industrial products will find use for this BLE module. Customers could also use large quantities for a development platform before finalizing BLE in the customer's end applications. The EZ BLE PRoC module has 21 pins with 16 signal connections. It supports SWD for flash programming. Cypress also provides an evaluation board on which this module will be mounted, and the evaluation board can either be plugged into a BLE pioneer kit or on a customer’s board for evaluation. Related collateral are populated on the website, including a datasheet, PRoC BLE datasheet (the PRoC BLE is the main IC inside the module), and a getting started application note which shows example projects for I²C, UART, or SPI based BLE projects. CYSMART tools are also included which include PC tools as well as an app that runs on android or IOS. These apps will also be supported for the EZ BLE PRoC module.

PTM פורסם ב: