Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
psoc creator getting started with ez-ble

PSoC Creator will be used with the EZ BLE to create firmware. PRoC modules will have a preconfigured view in PSoC Creator to develop, program, debug, and test. The latest Creator updates on the web are already supporting EZ BLE modules. BLE components and site creator are used to configure modules. One can select a profile, create GAP settings, and configure profile and GATT parameters in the component. The BLE component datasheet is included in the tool itself. This is a GUI-based tool to create and configure BLE protocol stack, and it is available as part of PSoC Creator. This is a pictorial view of the module; it is 10 mm by 10 mm by 1.8 mm in size. Height is also important for some volume constraint applications. Modules include shielding, which ensures signal, clocks, and crystals do not impact RF performance. Modules have crystals, passives, and a 2.4 GHz chip antenna. A 1.8 mm height includes PCB thickness. On the real side of the module, there is a 21 SMT process compatible signal, power, and group pins on three sides of the module. This ensures a module can be placed in the corner of an industrial design and will prevent any RF coupling issues. I/O supports GPIO, I²C, UART, SPI, PCBWM, I²S, or LCD Drivers.

PTM פורסם ב: