Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PSoC 4100 and 4200 Programmable System-on-Chip Slide 13

One example of the value of the programmable analog is the ADC differential Preamplifier Start project. In this project, the integration of an MCU and two discrete Op-amps in the differential preamplifier analog frontend is simplified using the PSoC Creator ADC Differential Preamplifier starter project and PSoC components. The customer can prototype quickly using the PSoC 4 Pioneer kit and an optional Arduino analog shield to create a PSoC one-chip solution.

PTM פורסם ב: