Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PSoC 4100 and 4200 Programmable System-on-Chip Slide 22

The PSoC 4 can also be used for user interfaces that includes CapSense buttons that just work because of Cypress’ rigorous engineering and testing. The CapSense component configuration tool and SmartSense auto-tuning simplify designs and eliminate manual tuning. PSoC 4 can drive and control LEDs, segment LCDs, and integrate light sensor AFEs for auto dimming. Again the PSoC 4 low-power mode saves power consumption. The PSoC 4 is a one-chip, reliable, easy-to-use low power solution for user interfaces.

PTM פורסם ב: