Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
output voltage adjustment

To increase the output voltage set point, connect an external resistor between the TRIM pin and Vo(-). To decrease the output voltage set point, connect an external resistor between the TRIM pin and Vo(+). The chart on the right of this page shows the maximum adjust range is ±10%; the TRIM pin should be left open if this feature is not used.

PTM פורסם ב: