Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Slew Rate Control

Slew rate control allows a switch to be turned on in a controlled fashion as not to overload the source voltage which may introduce droops or transients that would be detrimental to system behavior. Inrush currents are a combination of the capacitive load and needed system load current (ILoad). The controlled VOUT slew rate as shown on the right limits peak currents preventing a drop in VIN and mitigating the peak current.

PTM פורסם ב: