Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Fuse-Slide13

To prevent damage to converter components, the fuse current rating is selected with a large enough current capability so that the fuse will not open under steady state conditions, yet will open during an abnormal (excessive) overload or short-circuit condition. Usually this results in selecting a fuse to be 150% to 200% percent of the maximum steady state input current at maximum load and minimum line input voltage.

PTM פורסם ב: