Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Fuse-Slide5

There are two types of overcurrent events: an overload condition, which is simply drawing excessive current beyond the designed capacity of the circuit; and a short circuit or fault current, which is a much higher current than the normal circuit current (IN). Fuses serve two main purposes: to protect components, equipment and people from risk of fire and electric shock caused by overcurrent conditions; and to isolate subsystems from the main system once a fault has occurred.

PTM פורסם ב: