Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List Associated Content
Image of Efinix Trion® FPGA and How They Work - Slide5

Highlighted here are the package offerings and the corresponding hard blocks for the larger devices, the T55, T85, and the T120 devices. These devices and package offerings all have the DDR Memory controller enabled for x16 bit interface with the BGA576 enabling x32 bit wide data bus. Additionally, the BGA576 has three MIPI/CSI blocks enabled vs the two controllers on the BGA324 package. These devices highlight the scalability of the Quantum Architecture; in fact these devices are much larger than some other competitive solutions.

PTM פורסם ב: