Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
J10X-Slide1

The use of self-protecting charging resistors in the J10X series is recommended in order to handle typical malfunctions such as short-circuits or failure of the relay switch. In fault-free charging, these components act like a fixed ohmic resistor and limit the peak value of the charging current. In case of a malfunction, the temperature and inherent resistance of the PTC ceramic increases in line with the increased ohmic losses and limits the current to a safe operating level.

PTM פורסם ב: