Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List

High-power fixed resistors are generally employed to limit the current when charging capacitors. This is accompanied by technical risks. For example, if the capacitor short circuits or the relay has a malfunction, the resistors will be subjected to high power levels continually, which can lead to the destruction of the resistor and/or the system.

PTM פורסם ב: