Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
pgood
The MxL7704 offers two configurable Power Good outputs, PG1 and PG2. Each PGOOD flag can be monitored and assigned via the 400 kHz I²C interface. Two sequencing and PGOOD routing scenarios are shown. In the first example, PG1 goes high at approximately 7 ms (2 ms after Buck 4 reached 90% of its final value). PG2 is assigned to the LDO and to Bucks 1, 2, and 3. PG2 goes high 2 ms after the last of those rails, 1, reaches >90% of its final value, which in this case is Buck 1.
PTM פורסם ב: