Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
VLISI-Slide15

The design process starts with a requirement but there are optional approaches to a solution. The engineer can design and build the power system from discrete components; requiring at a minimum a micro-controller, some ADCs and DACS with the appropriate resolution and accuracy. Perhaps add some digital trim pots, several PWM controllers. If the requirement is for better than 1% accuracy, it is likely to need 0.1% precision resistors with good quality capacitors for the compensation network. It will also be necessary to allocate design time, a budget, test time, software development for the micro, board space and, if it is like most projects, more time and money than was originally requested to make it work properly.

PTM פורסם ב: