Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
VLISI-Slide9

The presentation will now discuss some VLSI device trends, covering a few types of devices and their attributes from a power perspective. The first of these are FPGAs. Many of these devices already specify dynamic power supply control and requirements for slew rate control and sequencing of the rails. Partial reconfiguration and the powering down of unneeded sections often requires turning on and off power rails. Accuracy of the applied voltages can be 1% or better and voltages can be 0.7V or lower.

PTM פורסם ב: