Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Advanced Energy Xgen Configurable Power Supplies - Slide6

This table summarizes the feature set for each output module. The Xgen output modules provide a considerable amount of functionality and versatility. J3 in the upper right hand column refers to signals on the 8 pin connector that are on each module. Most modules include Vtrim, Itrim, Inhibit, Enable and Power Good. Module Xg8 is a dual output module which has a four pin power connector to provide outputs V1 and V2. Modules Xg1 through Xg5 have both the Ishare dip switch and the Inhibit/Enable dip switch.

PTM פורסם ב: