Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Board-to-Board Mating Options

Vertical-to-vertical heights are the PCB-to-PCB mating face distances. For mating heights involving horizontal connectors, the dimension is taken from the total footprint of the connector; for example, the back edge of the SMT tails. The dimensions given in the table are for the connectors fully mated, but the product will perform with up to 1.5 mm separation, increasing the possible heights.

PTM פורסם ב:
PTM Updated on: 2025-06-16