Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List Associated Content
Single Piece Aluminium Construction

Female cable backshells are made of one piece of aluminium, with a nickel coating for corrosion protection. At the rear of the backshells, the exit has an extended collar with a raised lip. Braided outer sheath can be assembled, providing a consistent shield both over the connector and along the cables. A Band-It tie is recommended for use with these connectors, to assemble the braid to the collar. The lip then prevents the tightened Band-It tie from being pulled away.

PTM פורסם ב: