Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Why Use Flex Circuit? (cont’d.)

There is also an advantage in mated height, and the amount of clearance required above the connection. The mated height of a cable connector is higher than that of a SMT connector. The cables are vertical and need additional space to bend sideways to avoid the next item above the connection. The FPC connection is already at a right angle to the connection, and no additional height is required.

PTM פורסם ב: