Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
HR08D-Slide10

To mate the connector, simply push it onto the receptacle. To un-mate, rotate the locking collar and pull the plug back from the receptacle. Simplified mating is enabled by the alignment markings. Mating guide keys are provided at 3 points to prevent contact damage and provide the ability to blind mate these connectors when needed. Plug connector does not damage the receptacle contacts.

PTM פורסם ב: