Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
HR08D-Slide2

The HR08D series is a small, waterproof circular connector that has Push-on bayonet locking and is designed for harsh environments. It is oil-proof and waterproof and is rated to IP68. The series includes a feature that allows the cable orientation to be positioned in one of eight different directions. Each position is separated by 45° increments. There is a secure cable strain relief and is RoHS compliant.

PTM פורסם ב: