Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
zx-slide22

Eye pattern diagrams give detailed information about how the connector is handling the signal being sent through it. Normally, a good eye pattern is very “open” in shape but this depends on how much frequency is being applied.  As seen in this diagram, there is an excellent eye pattern at 480 Mbps (USB2.0 standard) with a 2.4m cable.

PTM פורסם ב: