Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
zx-slide24

This test data is showing the amount of insertion force required before, during and after a 10,000 cycle test. The insertion standard is 35 Newtons maximum. As can be seen from this test, the starting point is well below the maximum and insertion forces remain stable throughout the 10,000 cycles.

PTM פורסם ב: