Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
first wave trenchstop 5 page
On this slide and the following is Infineon‘s current TS 5 portfolio and ongoing portfolio extension. Infineon is currently offering the TS5 in three packages: the TO220, the TO220 FullPak, and the TO-247. The first box shows the 40 and 50 A devices without free wheeling diode. Infineon offers all devices in both variants, the F5 and H5 variant. The bottom box shows Infineon‘s devices with a free wheeling diode.
PTM פורסם ב: