Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
fam struct
The TS5 family structure and the different variants of the TRENCHSTOP5 technology. As mentioned before, Infineon offers the best-in-class TS5 technology currently in two variants. Additional two variants are in development and planned for 2014. As demonstrated on the left side of this slide, Infineon is offering the H5, a high-speed variant and the F5, a highest efficiency variant, shown on the right-hand side. In the lower box, one can see the R5 with monological integrated diode. This variant is currently in development, especially for Induction Heating applications and resonant topologies. Shown on the right side is the L5, the low Vce(sat) variant for Solar which is also under development.
PTM פורסם ב: