Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MicroModule Best Practices Slide 7
MicroModule is available in two actuator styles, either a Finger Disk or Mini-Joystick. Both actuator styles deliver simultaneous 360º control of direction and speed with the touch of a finger. All MicroModule pointing solutions are maintenance free and deliver “mouse” lifetimes in excess of five million actuations. To use MicroModule, place fingertip on the center of the actuator and rock it in the direction one wants to move. MicroModule has full 360º directional control. Use a light touch for precision movement, or increase the pressure to increase the speed of the cursor. The click buttons are located on either side of the actuator and operate like those on a conventional mouse. The left button on the MicroModule is used as the default primary button, the right button is used as the default secondary button. The customer can interchange the operation of the buttons in the Windows Control Panel (for left-handed users). To drag an item, simply press and hold the primary button while moving the cursor with the actuator, release the primary button to complete the drag operation. Some users find it easier to swap click buttons and use the right click as the primary button, allowing fore-finger cursor control with middle-finger clicking.
PTM פורסם ב: