Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
discretepower-vs-module-slide7

System designers will make trade-offs between cost, design effort and performance when selecting a power module. For systems with one to three power rails, designers may decide to use discrete regulators in order to save cost and meet the time to market schedule. However, as the number of power rails increases and the current rating increases, the design of the power subsystem becomes more challenging and requires significantly more design effort. To meet this challenge, designers may opt to use a power module solution. Designers will also consider the cost of ownership of a discrete design. The cost of ownership is the bill of materials (BOM) cost in addition to the power designer’s time required to design and test the design. Potential re-design changes, manufacturing, and assembly costs are additional expenses for discrete designs. The diagram on this slide shows how a power module can integrate many of the blocks of the discrete design shown earlier. A power module integrates the PWM controller, power MOSFETs, inductor, and compensation network into the package. The designer typically only needs to select the input and output capacitors, and a few resistors to complete a design. The only other consideration in a power subsystem design is the PCB layout.

PTM פורסם ב: