Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Industrial-Control-Slide9

In a large amount of industrial applications, the input voltage will be from a 24V rail. Stepping this down to a usable voltage for the analog circuitry in an efficient and easy-to-use way is very important. Generally, there will be at least two voltage rails required, maybe 3.3V and 2.5V, so a dual switcher like the ISL85033 is a great choice. Both channels will deliver 3A each, and if needed, the two rails can be tied together to get 6A. One of the advantages of using a dual switcher is the fact that both channels can be set to run 180° out of phase. This will reduce the input capacitance need. The part can be set to run at a frequency up to 2MHz, reducing the size of the external inductor and output capacitance.

PTM פורסם ב:
PTM Updated on: 2016-04-19