Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
MLCC-Slide6

The capacitance value of a capacitor is determined by four factors. The number of layers in the part, the dielectric constant and the active area are all directly related to the capacitance value. The dielectric constant is determined by the ceramic material (NP0, X7R, X5R, or Y5V). The active area is just the overlap between two opposing electrodes. The fourth factor, the dielectric thickness, is inversely related to the capacitance value, so the thicker the dielectric, the lower the capacitance value. This also determines the voltage rating of the part, with the thicker dielectric having a higher voltage rating than the thinner one. This is why the basic trade off in MLCCs is between voltage and capacitance.

PTM פורסם ב: