Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Image of KEMET's Aluminum Electrolytic Capacitors Slide 11

These are the potential failure modes of an aluminum electrolytic capacitor. Looking at the ESR increase as an example, earlier it was established that lower the ESR the better it is. A possible reason for an increased ESR could be a reduction in electrolyte or anode cathode foil capacitance drop. These are caused due to operating conditions or excessive thermal stress to name a few.

PTM פורסם ב: