Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Image of KEMET's Aluminum Electrolytic Capacitors Slide 6

The manufacturing process begins with slitting of the foil. This is where the foil is cut depending on the Capacitance value and dimensions. The foil and paper go into winding where its rolled into a cylindrical shape, after that the tabs are welded onto the deck. Once this is complete it goes into the impregnation chamber where the capacitor is soaked in electrolytes, so the separator paper can absorb the electrolytes. The capacitor is then put into a can and sealed. The aging process repairs the damaged parts of the dielectric where the foil was slit and the rated voltage is applied. Finally, the capacitor goes into standard testing such as ESR, capacitance and leakage current.

PTM פורסם ב: