Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Aluminum Electrolytic Screw Terminal Snap-In Capacitors Slide 1

Welcome to the KEMET Aluminum Electrolytic Screw Terminal and Snap-In Capacitors product training module. This presentation will provide an overview of Screw Terminal and Snap-In capacitors for industrial and power applications. It will discuss and highlight the selection tables and applications, the ways operating life is given in the datasheets and how that is used for estimating life in the user’s application. The tutorial will an example of how a more detailed life calculation is done for demanding power applications.

PTM פורסם ב: