Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
FilmCap-Slide13

The output converter typically does not draw a steady current. Rather, the current is in step with the IGBT switching. As the input converter cannot readily handle the current peaks, the DC bus voltage would have a significant ripple component which could adversely affect the operation of the system. It is necessary to place a capacitor of sufficient size on the DC bus to serve as a ripple smoothing filter. This capacitor is commonly called a DC link capacitor.

PTM פורסם ב: