Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Powering Devices in the Home

The term “Mains” or “Mains Voltage” refers to the electrical power that is delivered to homes and businesses and it is the form of electrical power that consumers use when they plug domestic appliances, televisions and electric lamps into wall outlets. Power in the home can be thought of as a network of multiple devices connected together on the same AC voltage line. Since these devices are on the same power network, the devices can affect one another. Therefore, it is important that there is proper isolation between the devices.

PTM פורסם ב: