Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Thermorite Performance (Heat Response)

Shown here is a chart of test data for heat response. Since the heat transmitting time varies depending on the difference between the heat source temperature and the operating temperature, the larger the operating temperature difference, the faster the response time. In addition, TRS has a larger material size than OHD, and because it uses aluminum material with high thermal conductivity, response time tends to be faster.

PTM פורסם ב: