Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
LCD-Slide4

The overall structure of an LCD is more than just a panel of liquid crystals. A basic LCD consists of two polarizers, two glass panels and liquid crystal that fits in between them. The front layer of glass is etched on the inside surface to form a template for the artwork to be shown by the liquid crystal. Liquid crystal bends light in response to the electric field.

PTM פורסם ב: