Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
IFJM-Slide4

The Class D Amplifier, or PWM Amplifier, has almost constant efficiency regardless of the output current in the practical region. However, the efficiency of the Class B Amplifier, or Analog Amplifier, is only 20% to 65% efficient. Therefore, the loss of the output stage can be greatly improved by the PWM Amplifier.

PTM פורסם ב: