Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
MAX11300 Programmable Mixed Signal IO Pt 3 Slide 15
The Munich GUI is used to create the sawtooth waveform for DAC on P4. Using a potentiometer, this level is fed to level-translator (P14) whose output (P3) is fed into an ADC (P13) where it is measured. Essentially this has created an adjustable pulse-width by using the potentiometer.
PTM פורסם ב: