Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
MAX11300 Programmable Mixed Signal IO Pt 3 Slide 4
The design engineer now connects the USB2PMB1 adapter to the MAX11300PMB via the PMOD connector and to the PC via the USB cable. The Munich GUI is opened, the configuration file is read and downloaded to the target MAX11300. The user can see that the ports are configured in the modes selected in the previous slide.
PTM פורסם ב: