Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Debug-Slide14

There are new benefits from the approach. First, it allows the entire application to be debugged as it executes with the actual embedded controller plugged in or soldered on the target board. Second, after the application is debugged, and even after it’s been deployed into the field, it can be reprogrammed without removing any components.

PTM פורסם ב: