Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Debug-Slide16

MPLAB ICD requires that a connector be added to the application, connecting to power and ground, the MCLR reset line, and the two pins for MPLAB ICD 2 communication. If you do not want to put a connector on the target then you could put pins on the target to connect with a “fling lead” assembly form MPLAB ICD 2.

PTM פורסם ב: