Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
EE-Slide9

The panels shown here highlight the compelling space saving and associated cost savings of the solutions highlighted. Compared to the original ISA interface implementation, the space savings using an SPI interface controller in comparison is 52% with an associated cost reduction of 34%. Compared to the Single-chip, integrated solution, the space savings is 68% and the approximate cost reduction is 51%.

PTM פורסם ב: